Search FAQs
Can the same RFID Authentication Card (EVRFIDKF10) be programmed into multiple EV chargers?
Issue:
Can the same RFID Authentication Card (EVRFIDKF10) be programmed into multiple EV chargers?
Product Line:
PTEVC - ELECTRICAL VEHICLE
Environment:
RFID enabled EVSE
Cause:
Single card use for multiple RFID enabled EV charging stations.
Resolution:
Yes, an RFID Authentication Card can be programmed into multiple EV chargers that are provided with the RFID Access function. Although the same card can be programmed into different ``slot numbers`` of different chargers, it is recommended to program a card into the same slot number of different chargers for better management purposes.
For instructions on how to program EVlink RFID enabled chargers please visit;
https://www.se.com/us/en/download/document/S1B23294/