{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an NF panel Series E1 with a Factory installed 400 amp LAL36400 Main breaker, be converted to a Main lug panel?
Issue:
Can an  NF panel with these characteristics be converted to a Main lug panel?
Series E1
Factory 400Amps LAL36400 Main breaker factory installed

Product Line:
NF Panelboard

Environment:
Application

Cause:
Field Changes

Resolution:
The main breaker kit should remain in place so the panel will utilize the same box and trim. The following parts will be required per panel:

(1) NFALM4 Main Lug Kit
(1) cover plate for the main breaker dead front
NOTE: THIS DOES NOT INCLUDE INTERIORS SUPPLIED W/ AN LC MAIN BREAKER.

Note: Revision 05/2017:
A cover plate for the hole in the main breaker dead front, formerly part number 80103-079-02, is obsolete and no longer available.  Consider having a local metal fabricator custom-make something to replace it.

Schneider Electric Canada