{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are manual transfer equipment or generator interlock kits available for older load centers that used a vertically mounted main breaker?
Issue:
Product Selection

Product Line:
QO Load Center Accessory

Resolution:
No, manual transfer equipment kits or generator interlock kits were not available until around 2000 and later and are not available for older load centers or load centers with a vertically mounted main breakers or branch breakers.

NOTES:
1) The manual transfer equipment and generator interlock kits are designed for the more current series G and S load centers only.
2) The manual transfer equipment kits or generator interlock kits are not available for the older Homeline load centers that used a 4 pole type main breaker (e.g. the HOM2150 or HOM2200).
3) The manual transfer equipment kits were only designed for the current QO load centers, NOT Homeline.

Schneider Electric Canada