{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the Part Numbers of the Auxiliary Contacts and Power Pole Adder for MD3304X and MD3604X Motor Disconnects?
Issue:
Need to know what available auxiliary contacts are compatible for the MD motor disconnect switches.

Product Line:
Disconnect Switches

Environment:
MD Motor Disconnect Switches

Resolution:
MDSAN20 - 2 N.O. auxiliary contact module
MDSAN11 - 1 N.O. and 1 N.C. auxiliary contact module
MDS30P - 30 A add on power pole

Maximum of one power pole adder (left side) and 2 auxiliary contacts can be installed per switch.

Schneider Electric Canada