{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the "O" ring gasket for the external operator on the Class 2510 Type MBA, MBW, MCA and MCW manual starter?
Issue:
Checking on the part number for the "O" ring gasket for the external operator on the Class 2510 Type M Series C manual starters.

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
2510 Type M Manual Starters

Resolution:
The "O" ring part number is 29206-30840.

Schneider Electric Canada