{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is included with the HOME250SPA Homeline spa pack?

Issue:
Product Design Features

Product Line:
Homeline Load centers

Resolution:
The HOME250SPA consists of an HOM250GFI ground fault breaker installed in an HOM2-4L50R, NEMA 3R (outdoor) metallic enclosure. The HOM2-4L50R enclosure is not merchandised separately.

See attached instruction bulletins for more information.

Schneider Electric Canada

Attachment(s)

Load Center Instruction Bulletin.pdfLoad Center Instruction Bulletin.pdf [183.46 KB]
2 pole HOM-GFIs.pdf2 pole HOM-GFIs.pdf [329.34 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: