{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What control power transformer is supplied with kit number 9999CPT1D1?
Issue:
Control Power Transformer kit components

Product Line:
Industrial Control

Environment:
Type T and Type FT

Resolution:
This is a pre-wired 9070TF100D1 welded to a special mounting plate.
NOTE: The 9999CPT1D1 is not for use in the Series K and later 8538/8539 combination devices. Use the standard 9070TF100 transformers.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: