Search FAQs
Are individually mounted enclosures available for the PowerPact H and J frame circuit breakers?
Issue:
What are the available enclosures for Powerpact H and J frame breakers?
Product Line:
Powerpact Breakers
Resolution:
Yes, below are the options for the Powerpact H and J frame enclosures. Please read all applicable footnotes.
What are the available enclosures for Powerpact H and J frame breakers?
Product Line:
Powerpact Breakers
Resolution:
Yes, below are the options for the Powerpact H and J frame enclosures. Please read all applicable footnotes.
- [9] Rated for 240 Vac maximum. Short circuit current rating is 25 kAIR at 240 Vac.
- [10] Accepts standard 80% rated circuit breakers only. Not rated for 100% rated circuit breakers.
- [11] Use copper conductors only.
- [12] Rated 480 Vac maximum. Short circuit current rating is 18 kAIR at 480 V.
- [13] For conduit entry through the top end wall use one of the following Square D conduit hubs: A200L for 2.00 in., A250L for 2.50 in., A300L for 3.00 in., A350L for 3.50 in. or A400L for 4.00 in.
- [14] Add suffix BE if no knockouts are required on the end walls.
- [15] For access to the circuit breaker’s standard, ammeter or energy trip unit panel/LCD, add suffix T.
- [16] For 200% neutral use copper wire only.
- [17] Complete rating is NEMA 3, 3R, 4, 4X, 5, and 12.
- [18] For NEMA 3R applications, remove drain screw from bottom endwall.
- [19] Add suffix VW for visibility to the standard, ammeter or energy trip unit of the PowerPact circuit breaker.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: