{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the 380 volt replacement coil for an 8502A Contactor?
Issue:
8502A 380V Coil replacement

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8502A Obsolete contactors

Resolution:
The coil numbers were 31012-400-58 for 60hz and 31012-400-60 for 50 hz. Both of these coils are obsolete and no longer available. Series A coils are also obsolete and no longer available. This also applies to all 8536A, 8702A, 8736A and 8810A, devices. For enclosed devices, the series information is based on device and not enclosure

Schneider Electric Canada