{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between the PK4FL and PK22FL?
Issue:
The difference between the PK4FL and PK22FL.

Product Line:
PTFDS -  FD  enclosure systems

Resolution:
The older PK4FL has flat ears on the backside. Through these are screw holes and screws attach the lock to elevated tabs or brackets on the rear of the trim. The PK22FL has nibs on the back that fasten via screws into flat pieces on the rear of the trim .

Picture showing each of the part numbers to show the difference

NOTE: It is a PK4FL if built before 11/1997 and a PK22FL if built after 11/1997.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: