{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is a replacement copper lug for a main lugs HCN I-Line panel ?

Issue:
Is there a replacement copper lug for a main lugs HCN I-Line panel ?

Product Line:
Panelboards

Environment:
I-Line Power Distribution Panelboard - HCN

Resolution:
Use a  80048-002-01 copper lug for 2 - #2 thru 600kcmil

Below is the terminal data for all of the panelboards found on page 9-40 in Digest 177, Section 9. Table 9.187 shows the terminal data for the phase and neutral lugs on main lug panels. Table 9.188 shows the standard terminal for main breaker available for ILINE panelboard (please see page 7-41 of Digest 177, Section 7 or page 3-28 of the Supplemental Digest 177, Section 3 for other terminal options for given breakers).

Standard Mechanical Lugs—Main Lugs

AmpLug Wire RangeWire Range Wire Bending Space per NEC Table 373-6
225 Aone #6–300 kcmil Al or Cuone #6–300 kcmil Al or Cu
400 Atwo #2–600 kcmil Al or Cuone #2–600 kcmil Al or Cu
600 Atwo #2–600 kcmil Al or Cutwo #2–500 kcmil Al or Cu
800 A(4) 3/0–750 kcmil Al or Cu(3) 3/0–500 kcmil Al or Cu
1200 A(4) 3/0–750 kcmil Al or Cu(4) 3/0–500 kcmil Al or Cu


Standard Mechanical Lugs—Main Circuit Breaker

AmpCircuit Breaker TypeLug Wire RangeWire Range Wire Bending Space per NEC Table 373-6
100 AFA, FH, FIone #14-1/0 Al or Cuone #14-1/0 Al or Cu
150 AHD, HG, HJ, HLone #14-3/0 Al or Cuone #14-3/0 Al or Cu
225 AKIone #4-300 kcmil Al or Cuone #4-300 kcmil Al or Cu
250 AJD, JG, JJ, JLone #1/0-#4/0 Al or Cuone #1/0-300 kcmil Al or Cu
LX, LXI, LEtwo #1-350 kcmil Al or Cutwo #1-350 kcmil Al or Cu
400 ALA, LHone #1-600 or two #1-250 kcmil Al or Cuone #1-600 kcmil Al or Cu
600 ALC, LI, LX, LXI, LEtwo 4/0-500kcmil Al or Cutwo 4/0-500kcmil Al or Cu
800 AMG, MJ, PG, PJ, PLthree 3/0-500 kcmil Al or Cuthree 3/0-500 kcmil Al or Cu
1200 APG, PJ, PL, RGC, RJC, RLCfour 3/0-500 kcmil Al or Cufour 3/0-500 kcmil Al or Cu

Schneider Electric Canada