{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the U-Line controllers DIN Track mountable?
Issue:
Does the LUB12, LUB32, LUB120, LUB320, and LU2B12, LU2B32 power base din rail mount?

Product Line:
IEC Contactors and Starters

Environment:
Tesys U Line Motor Starters

Cause:
Installation

Resolution:
Yes, requires DIN 3 (35 mm) rail, Examples of suggested rail listed below:
35 mm, 7.5 mm deep, 2000 mm long - NSYSDR200BD.(Steel rail with zinc chromate film)
35 mm, 15 mm deep, 2000 mm long - NSYDPR200T. (Steel rail with zinc chromate film)


Schneider Electric Canada