{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the blanks extensions HLW4EBL and HLN4EBL used for?
Issue:
HLW4EBL and HLN4EBL characteristics

Product Line:
Panelboards

Environment:
I-Line Power Distribution Panelboar

Resolution:
These are blank extensions, which are added on to the end of a breaker to fill in the additional space in a deadfront to prevent exposure of the bus.
HLW4EBL is to be added onto the end of H and J frame breakers with Micrologic 5 or 6 trip units mounted on the wide side of an I-line panelboard.
HLN4EBL is to be added onto the end of H and J frame breakers with Micrologic 5 or 6 trip units mounted on the narrow side of an I-line panelboard.

Schneider Electric Canada