{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the terminal pad hole size for the power and motor cable lugs on the ATS48C14Y or ATS48C17Y?

Issue:
ATS48C14Y or ATS48C17Y terminal pad hole size.

Product Line:
Altistart 48  ATS48

Environment:
All

Cause:
N/A

Resolution:
The hole dimension is 9 mm as shown in the Altistart 48 Y-Range Soft Start Controllers Instruction Bulletin S1A37491.
image.png

Schneider Electric Canada