Issue:
Need to know the material of the enclosure that is on the MD3304X and the MD3604X
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
MD Motor Disconnect Switches
Resolution:
The enclosure is Non-metallic, rated for both indoor and outdoor use, is UV and corrosion resistant (Types 1, 3, 3R, 4, 4X, and 12). See the Instruction Bulletin IS536778.
Need to know the material of the enclosure that is on the MD3304X and the MD3604X
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
MD Motor Disconnect Switches
Resolution:
The enclosure is Non-metallic, rated for both indoor and outdoor use, is UV and corrosion resistant (Types 1, 3, 3R, 4, 4X, and 12). See the Instruction Bulletin IS536778.