Issue
What is the replacement black handle for a LK3QU3 disconnect rated NEMA 1 or NEMA 12?
Product Line
Non Fused disconnect
Environment:
GS1 and LK3
Cause
Repair, replace or selection
Resolution
For the non-defeatable black handle we offer the LK3AH150. For the defeatable black handle we used the LK3AH170.
What is the replacement black handle for a LK3QU3 disconnect rated NEMA 1 or NEMA 12?
Product Line
Non Fused disconnect
Environment:
GS1 and LK3
Cause
Repair, replace or selection
Resolution
For the non-defeatable black handle we offer the LK3AH150. For the defeatable black handle we used the LK3AH170.