{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Square D have any fused or Non-fused 1000Vdc photovoltaic disconnect switch?
Issue:
Product Design Features

Product Line:
HD TYPE SWITCHES

Environment:
1000V DC switches

Cause:
Application

Resolution:
No, All of the 1000V DC switches have been obsoleted and are no longer available with no replacements. - Schneider Electric currently only offers 600VDC rated safety switches. For 600VDC applications please see our current Heavy Duty Safety Switches.

The below switches were the catalog numbers of the 1000V DC that were offered by Square D/Schneider Electric, but are no longer available.
  • REHU393IP - 100A 3 Pole
  • REHU394IP - 200A 3 Pole
  • REHU493IP - 100A 4 Pole
  • REHU494IP - 200A 4 Pole

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: