{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for a drum switch, rated 115 V, 1.5 HP, and weather resistant?
Issue
Weather resistant drum switch

Product line
drum switches

Environment
2601

Cause
Product selection

Resolution
Suggested part number 2601AW2 which is rated NEMA 4 and is water tight.

Schneider Electric Canada