{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a 2 pole NC contactor rated for 60 Amps?
Issue
2NC Contactor selection

Product Line
Contactors

Environment
Tesys D-line and 8903S Lighting Contactors

Resolution
No. but the customer can use an LC1D80008G7 and only use the NC contacts. Alternatively a type 8903SP lighting contactor cold be purchased with the addition of the 9999SB25 NC power poles.

Schneider Electric Canada