{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How many poles can be added to a MD3604X?

Issue:
Can power poles can be added to a MD3604X?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
MD Motor Disconnect Switches

Resolution:
Schneider Electric does not have a 60A power pole adder. However, it is possible to add 1 MDS30P power pole to the left side.

***NOTE*** The power pole is only rated 30A -- not 60A -- so it will be like adding a 30A NO auxiliary contact block.

Schneider Electric Canada