Search FAQs
What is the replacement for an FAL/FAP Mag-Gard MCP (motor circuit protector)?
Issue:
Replacement for FAL/FAP MCP
Product Line:
Legacy motor circuit protector
Environment:
FAL MCP
Resolution:
NOTE: Dimensions are different and the replacements listed below may not fit properly in the original equipment.
You will need to verify the type of equipment the original breaker is installed in before ordering. If MCC, replace complete bucket.
Replacement for FAL/FAP MCP
Product Line:
Legacy motor circuit protector
Environment:
FAL MCP
Resolution:
NOTE: Dimensions are different and the replacements listed below may not fit properly in the original equipment.
You will need to verify the type of equipment the original breaker is installed in before ordering. If MCC, replace complete bucket.
- FAP- or FHP- crosses to HJP-
- FAF- or FHF- crosses to HJF-
Breaker | Amps | Trip Range | Replacement | Trip Range |
FAL3600311M | 3 | 8-28 | HJL36030M71 | 9-325 |
FAL3600712M | 7 | 18-70 | HJL36030M71 | 9-325 |
FAL3601513M | 15 | 50-180 | HJL36030M71 | 9-325 |
FAL3603013M | 30 | 50-180 | HJL36030M71 | 9-325 |
FAL3603015M | 30 | 100-350 | HJL36030M71 | 9-325 |
FAL3605014M | 50 | 75-260 | HJL36050M72 | 84–546 |
FAL3605016M | 50 | 150-580 | HJL36050M72 | 84–546 |
FAL3610016M | 100 | 150-580 | HJL36100M73 | 180–1040 |
FAL3610018M | 100 | 300-1100 | HJL36100M73 | 180–1040 |
FAL3615024M | 150 | 450-1100 | HJL36150M74 | 348–1690 |
Breaker | Amps | Trip Range | Replacement | Trip Range |
FHL3600311M | 3 | 8-28 | HJL36030M71 | 9-325 |
FHL3600712M | 7 | 18-70 | HJL36030M71 | 9-325 |
FHL3601513M | 15 | 50-180 | HJL36030M71 | 9-325 |
FHL3603013M | 30 | 50-180 | HJL36030M71 | 9-325 |
FHL3603015M | 30 | 100-350 | HJL36030M71 | 9-325 |
FHL3605014M | 50 | 75-260 | HJL36050M72 | 84–546 |
FHL3605016M | 50 | 150-580 | HJL36050M72 | 84–546 |
FHL3610016M | 100 | 150-580 | HJL36100M73 | 180–1040 |
FHL3610018M | 100 | 300-1100 | HJL36100M73 | 180–1040 |
FHL3615024M | 150 | 450-1100 | HJL36150M74 | 348–1690 |