Search FAQs
What is the replacement for a KAL or KHL Mag-Gard motor circuit protector?
Issue:
KAL Mag Gard replacement
Product line:
Circuit breakers
Resolution:
The replacement is in the following table.
Note that the dimensions are different and the replacement may not fit properly in the original equipment.
KAL Mag Gard replacement
Product line:
Circuit breakers
Resolution:
The replacement is in the following table.
Note that the dimensions are different and the replacement may not fit properly in the original equipment.
Breaker | Trip | Cross | Trip |
KAL3625021M | 400 - 800 A | JJL36250M75 | 684 – 2500 A |
KAL3625022M | 500 - 1000 A | JJL36250M75 | 684 – 2500 A |
KAL3625025M | 625 - 1250 A | JJL36250M75 | 684 – 2500 A |
KAL3625026M | 750 - 1500 A | JJL36250M75 | 684 – 2500 A |
KAL3625029M | 875 - 1750 A | JJL36250M75 | 684 – 2500 A |
KAL3625030M | 1000 - 2000 A | JJL36250M75 | 684 – 2500 A |
KAL3625031M | 1125 - 2250 A | JJL36250M75 | 684 – 2500 A |
KAL3625032M | 1250 - 2500 A | JJL36250M75 | 684 – 2500 A |
KAL3625033M | 1500 - 3000 A | JJL36250M75 | 684 – 2500 A |
Breaker | Trip | Cross | Trip |
KHL3625021M | 400 - 800 A | JJL36250M75 | 684 – 2500 A |
KHL3625022M | 500 - 1000 A | JJL36250M75 | 684 – 2500 A |
KHL3625025M | 625 - 1250 A | JJL36250M75 | 684 – 2500 A |
KHL3625026M | 750 - 1500 A | JJL36250M75 | 684 – 2500 A |
KHL3625029M | 875 - 1750 A | JJL36250M75 | 684 – 2500 A |
KHL3625030M | 1000 - 2000 A | JJL36250M75 | 684 – 2500 A |
KHL3625031M | 1125 - 2250 A | JJL36250M75 | 684 – 2500 A |
KHL3625032M | 1250 - 2500 A | JJL36250M75 | 684 – 2500 A |
KHL3625033M | 1500 - 3000 A | JJL36250M75 | 684 – 2500 A |
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: