{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can 90 degree celsius wire be used on a circuit breaker?
Issue:
Is it acceptable to use wire with 90 deg. C insulation on a molded case circuit breaker?

Product Line:
All MCCBs; legacy and Powerpact

Resolution:
It is acceptable to use conductors with a higher insulation rating than what is marked on the breaker, but the ampacity must be based on the conductor temperature rating marked on the breaker. So, circuit breakers marked for use with 75 deg. C rated conductors may be used with conductors rated for 90 deg. C if the conductors are sized per their 75 deg. C ampacity.

Schneider Electric Canada

Attachment(s)
Wire Terminations 0110DB9901R2-02.pdf [82.43 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.