{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the terminal temperature rating on Powerpact M, P, and R frame circuit breakers?
Inquiry:
What is the terminal temperature rating on Powerpact MG, MJ, PG, PJ, PK, PL, RG, RJ, RK, and RL circuit breakers?

Product Line:
Circuit Breakers

Resolution:
The termination rating for these circuit breakers is 75 deg. C.
This means that if terminated with cable, the insulation rating must be rated for 75 deg. C or greater, and the conductor size must be based on its 75 deg. C ampacity.
Circuit breakers rated above 100 A are required to be suitable for 75 deg. C wire and do not need to be so marked.

Schneider Electric Canada