Search FAQs
Can a 90degC conductor be used in a QED 2 or QED 6 switchboard?
Issue:
Use 90 deg C wires in a switchboard
Product Line:
Switchboards
Environment:
QED
Speed
CMM
PZ4
Resolution:
90degC conductors can be used for 80% and 100% applications but must be sized for 75 degC cable capacity. However, 90 degC wire should be used in 100% applications but still need to sized to 75degC cable capacity.
See bulletin 2700DB0203
Released for:Schneider Electric Canada
Explore more
Category:
Range:
Explore more
Category:
Range: