{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What ambient conditions are acceptable for operation and storage of Powerpact M, P, and R frame circuit breakers?
Inquiry:
What considerations must be made for ambient temperature, humidity, altitude, and vibration when storing or operating Powerpact M, P, and R frame circuit breakers?

Product Line:
Circuit Breakers

Resolution:
Powerpact circuit breakers are suited for use:

At ambient temperatures between -13°F (-25°C) and 158°F (70°C). Operating the breaker above 104F (40C) may require derating or overbussing the circuit breaker; see attachment for details.
At altitudes less than or equal to 13,000ft. (3900 meters).  At altitudes > 6600 ft. (2000 m), rerating factors apply; see attachment for details.
It is recommended that the equipment be cooled or heated to the proper operating temperature and kept free of excessive vibration and dust, and be protected from water intrusion and condensation.
See attachment for vibration, humidity, and storage recommendations.

Schneider Electric Canada

Attachment(s)
Operating Conditions for Powerpact M P R 0612CT0101.pdf [82.31 KB]