{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can wire pulling compound be used for the conductors of an isolated power system?

Issue:
Installation/startup

Product Line:
Hospital Isolated Power Systems

Environment:
NFPA99,NEC517.160


Resolution:
Wire pulling compound should not be used.

NEC 517.160 (A) (6) Wire-Pulling Compounds.
Wire-pulling compounds that increase the dielectric constant shall not be used on the secondary conductors of the isolated power supply.
Informational Note No. 1: It is desirable to limit the size of the isolation transformer to 10 kVA or less and to use conductor insulation with low leakage to meet impedance requirements.
Informational Note No. 2: Minimizing the length of branch-circuit conductors and using conductor insulations with a dielectric constant less than 3.5 and insulation resistance constant greater than 6100 megohm-meters (20,000M ohm-feet) at 16°C (60°F) reduces leakage from line to ground, reducing the hazard current.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: