{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can a GFCI be used on an isolated power system?

Issue:
Using a GFCI on an Isolated Power System

Product Line:
Hospital Isolated Power Systems

Environment:
NFPA 99, NEC 517.160

Resolution:
GFCI devices should never be connected to an Isolated Power System. GFCIs will not operate properly and can result in unwanted ground connection in the Isolated Power System.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: