Goals and Symptoms
Getting error E7701 on LXM32 and unable to reset
Facts and Changes
LXM32
Causes and Fixes
E7701:System error: Timeout during connection to power stage.
You can try to update the firmware if you have an older revision.
This is an error in the power stage so most of the time, you need to send the LXM32 back for replacement