{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can 800 series modules be used with Unity software?

Yes. *800 series modules can be used as remote I/O drops in a Quantum or larger M580 systems with the Unity software. For more information on which modules are compatible, and for configuration information please consult the Modicon Quantum 800 Series I/O Modules with Unity Reference Manual.


*Note: Although compatible, the 800 series family of  I/O is obsolete. Please consider alternatives offered in the Quantum or BMX families of IO .

Schneider Electric Canada