Search FAQs
What is the Country of Origin for my ION and PowerLogic meters?
Issue
User is unable to find documentation on the Country of Origin
Product Line
PM800, PM8000 series, PM5000, CM4000, ION7550, ION7650, ION8650, ION8800, ION7400
Environment
Country of Origin
Resolution
Meter | Description | Country of Origin |
METSEPM8240 | PM8000 Power Meter Panel Mount With Display | Mexico |
METSEPM82401 | PM8000 Power Meter Panel Mount With Display | Mexico |
METSEPM8243 | PM8000 Power Meter DIN Rail No Display | Mexico |
METSEPM8244 | PM8000 Power Meter DIN Rail with Remote Display | Mexico |
METSEPM89M0024 | PM8000 Analog I/O Module, 2 Out, 4 In | China |
METSEPM89M2600 | PM8000 Digital I/O Module, 2 Relay, 6 DI | China |
METSEPM89RD96 | PM8000 Remote Display with 3M Cable | China |
METSEPM8RDHWK | PM8000 Remote Display Hardware Replacement | China |
METSEPM8HWK | PM8000 Power Meter Hardware Replacement | Canada |
METSEPM8000SK | PM8000 Sealing Kit | Canada |
METSEPMAK | PM Mounting Adapter Kit | Canada |
Meter | Country of Origin |
DM6200 | India |
Meter | Country of Origin |
PM210 | Mexico |
PM710 | US |
PM750 | Mexico |
PM800 | Mexico |
PM1200 | India |
Meter | Country of Origin |
PM5000 | India |
Meter | Country of Origin |
CM4000 | Mexico |
CM4000T | Canada |
Meter | Country of Origin |
ION7400a | See below |
ION7550 | Canada |
ION7650 | Canada |
ION8650 | Canada |
ION8800 | Canada |
Meter | Country of Origin |
E5600 | Canada |
EM3500 | US |
EM4800 | Canada |
Meter | Country of Origin |
EGX100 | India |
EGX300 | India |
EBX200/Com'X200 | Germany |
Meter | Country of Origin |
Enercept | US |
Meter | Country of Origin |
BCPM | US |
Meter | Country of Origin |
MCM | US |
Meter | Country of Origin |
ION Setup Software | Canada |
a: The ION7400 meter is assembled in Canada, the specific country of origin is dependent on the serial number on the meter. Contact Technical Support with the serial number, and Tech Support will request the Hardware team for the country of origin.
Note: Contact technical support if the official documentation specifying the Country of Origin is needed.
For more information, contact Schneider Electric Technical Support from the Customer Care Center at (888)-797-6468 or pmo.support@se.com
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: