{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the current part numbers for the EM4800 product range?
Issue
Part numbers have been updated for the EM4800 series.

Product Line
EM4800 Series

Environment
Meter and Accessory Part Numbers

Cause
A reference is useful for comparing old (prior to June 2011) and new part numbers. Note that the form factor and measurements available are not affected by the transition in part numbers, but customers will receive additional features in the new part numbers, as compared to the old parts. Not all part numbers are launched in all countries due to differences in branding (Square D (SqD) and Schneider Electric (SE)), control power voltage and calibration frequency.

Resolution
Old Part Number New Part Number Description
E488010SQDMETSEEM48801680 mA CTs, 120 V CP, 60 Hz SE
E488010SQD METSQEM488016 80 mA CTs, 120 V CP, 60 Hz SqD
E488020SQDMETSEEM488025 80 mA CTs, 240 V CP, 50 Hz SE
None METSEEM48802680 mA CTs, 240 V CP, 60 Hz SE
E480510SQDMETSEEM4805165 A CTs, 120 V CP, 60 Hz SE
E480510SQDMETSQEM4805165 A CTs, 120 V CP, 60 Hz SqD
E480520SQD METSEEM4805255 A CTs, 240 V CP, 50 Hz SE
NoneMETSEEM4805265 A CTs, 240 V CP, 60 Hz SE
E483310SQDMETSEEM4833161/3 V CTs, 120 V CP, 60 Hz SE
E483310SQDMETSQEM4833161/3 V CTs, 120 V CP, 60 Hz SqD
E483320SQDMETSEEM4833251/3 V CTs, 240 V CP, 50 Hz SE
None METSEEM4833261/3 V CTs, 240 V CP, 60 Hz SE
METSEEM48RD*EM4800 remote display, SE
METSQEM48RD*EM4800 remote display, SqD
METSECTSHORTCT Shorting Module
METSECTTERMCT Termination Module
METSECT80XXXSolid-core CTs for METSEEM4x8xxx meters

* See FA212613 for additional details on remote display

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.