Search FAQs
What is the recommended wire length for extending current transformers (LVCT, SCCT)?
Issue:
The user would like to extend the leads on a low voltage or split core current transformer.
Product Line:
Low Voltage and Split Core Current Transformers
Environment:
Current Transformers
Cause:
The monitoring source may be beyond the reach of the existing LVCT or SCCT leads and needs to be extended.
Resolution:
Powerlogic LVCT, both 1Vac and 1/3 Vac current transducers
- Up to 100 feet using the same wire gauge size. To avoid noise, use twisted pair wire for 18 AWG and above.
Powerlogic 3090 Split Core Current Transformers (SCCT):
*Note: Below ratings are with 14 gauge wires
*Note: Ideally the lead extension should be twisted
- For CT amperage 200 Amps and below: up to 20 feet
- For CT amperage 300 - 400 Amps: up to 35 feet
- For CT amperage 500 - 600 Amps: up to 60 feet
- For CT amperage 800 Amps and greater: up to 100 feet.
To find the cut sheet for the LVCT and/or 3090SCCT series CTs, please refer to FA212730.