{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the ION8650 UL listed?
Issue:
When looking at the UL listing for various ION meters, it may be noticed that the ION8xxx series socket meters are not UL listed.
Product Line:
ION8650 and ION8xxx series power meters
Environment:
Utility meter offering
Cause:
Some projects require that all equipment used on the project is UL listed.
Resolution:
These meters are not UL listed. The reason is that the meters are designed for utility metering and utilities typically do not require UL listing.

Schneider Electric Canada