{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for a 1600A or above disconnect switch in a NEMA 3R enclosure?

Issue:
Selecting a part number for a 1600A or above, disconnect switch in a NEMA 3R enclosure

Product Line:
Switchboard

Environment:
QED 2, BP switch

Resolution:
Product will need to be configured as a N3R switchboard with a Bolted-Pressure switch.
This can be done using QuoteFast, EQM, or product selectors. Contact your local distributor for a quotation.
Be sure to confirm the system voltage because a ground fault relay is needed for a 480/277v switch for service entrance.

Schneider Electric Canada