Issue:
Product Design Features
Product Line:
Heavy Duty Safety Switch
Resolution:
Provisions for installing Class J fuses are included in 30 - 400 A, 600 V and 100 - 400 A, 240V, fusible heavy duty safety switches. Conversion to Class J fuse spacing requires relocating the load side fuse base assembly (or assemblies where applicable) from the standard Class H or R fuse location to an alternate position as marked in the switch enclosure. Switches rated 600 A, 240V or 600V, require the addition of an adapter kit, catalog number H600J.
PLEASE MAKE SURE NEVER TO WORK ON ENERGIZED EQUIPMENT.