{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the selection in the 22mm and 30mm pendant station?

Article available in these languages: Spanish

Issue:
What type of products are offered in a Pendant Station ?

Product Line:
XAR eXL Hoist, XACA-2, XACA, 9001BW and 9001SKYP Pendant Stations

Environment:
US product

Cause:
Specification and Rating information

Resolution:
There are about 5 type of pendant offered: XAR eXL Hoist Wireless ; XACA2-Button Pistol Grip Pendant ; XACA0 General Purpose Pendant 2 to 12 buttons; the Class 9001BW 2-Button Pendant and the 9001SKYP the Heavy Duty Pendant 2 to 10 buttons.
Additional information about ratings and specifications can be found in Pendant Stations Type 9001BW, 9001SKYP, XACA, and XAR eXL Hoist Wireless catalog which can be downloaded here: http://download.schneider-electric.com/files?p_Doc_Ref=9001CT1001

Schneider Electric Canada