{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

For Powerpact breakers, will the direct mounted rotary handle fit onto an existing door mounted rotary handle shaft?

Issue:
For an existing breaker with a door-mounted rotary handle, if the rotary handle needs replacing, will the direct-mounted rotary handle fit into the same place?

Product Line:
Circuit Breakers

Resolution:
No, the direct mounted rotary handle will not fit onto the shaft of an existing door mounted rotary handle. The reason is due to how they are installed onto the breaker.

DIRECT MOUNTED ROTARY HANDLE DOOR MOUNTED ROTARY HANDLE
Consists of one part: Rotary Handle                                                                        Consists of three parts: Rotary Handle, Shaft, Base
Attaches to the face of the breaker itself (no shaft)                                                           Attaches to panel door, shaft connects to breaker
Fixed handle Door mounted handle



Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: