Issue:
Will the LU2MBO reverser module fit in the current LUB12 and LUB32 U-line starters?
Product Line:
IEC Telemecanique starters
Environment:
Tesys U line Starters
Cause:
Selecting a reversing U-Line starter
Resolution:
The new line of Tesys U starters do not have removable terminals on the botom therefore the LU2MBO reverser module will not fit. The LU2B12 and LU2B32 come with reverser modules, and the LUB120 and LUB320 come without terminal blocks for use with the reversing modules or communication modules.
Released for:Schneider Electric Canada
Issue:
Will the LU2MBO reverser module fit in the current LUB12 and LUB32 U-line starters?
Product Line:
IEC Telemecanique starters
Environment:
Tesys U line Starters
Cause:
Selecting a reversing U-Line starter
Resolution:
The new line of Tesys U starters do not have removable terminals on the botom therefore the LU2MBO reverser module will not fit. The LU2B12 and LU2B32 come with reverser modules, and the LUB120 and LUB320 come without terminal blocks for use with the reversing modules or communication modules.
Released for:Schneider Electric Canada