{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
On the class 8536 type S size 3 and 4 with form Y59 do we use type E furnas thermal units?
Issue:
On the class 8536 type S size 3 and 4 with form Y59 do we use type E furnas thermal units?

Product Line:
NEMA Type S Motor Starters (8536 8736 8606)

Environment:
NEMA Starters

Cause:
On the class 8536 type S size 3 and 4 with form Y59 do we use type E furnas thermal units?

Resolution:
The size 3 and 4 8536 type S starters with form Y59 do use a furnas overload block and therefore use furnas type E thermal units. Which are now Obsolete

Schneider Electric Canada