{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the XW Equalization Period?

XW Equalization Period
Equalization period is limited to 1 hour.
The following lists the devices that comply with this parameter
Conext XW Hybrid Inverter/Charger
Conext XW MPPT60-150
Conext XW MPPT80-600

NOTE:If specific gravity does not indicate cells are equal after 1 hour, then additional equalization cycles must be initialized.
Warning:Excessive equalization can cause loss of fluid and damage to the batteries. Equalization should not be performed while unattended.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.