Search FAQs
How is I-Line phasing designated in circuit breaker catalog numbers?
Issue:
Determine the phase connection of I-Line breakers in the I-Line Panelboard
Product Line:
Panelboards and Molded Case Circuit Breakers
Resolution:
Below is a table that shows the catalog number suffixes for I-line breakers.
Table 9.121 represents the number system for Powerpact breakers.
Table 9.122 represents the number system for the older Legacy breakers.
The absence of a phase option suffix after a 3 pole catalog number will result in an ABC phase connection.
![Table 9.121 Table 9.121](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zq8DQAQ&oid=00DA0000000abSm)
Determine the phase connection of I-Line breakers in the I-Line Panelboard
Product Line:
Panelboards and Molded Case Circuit Breakers
Resolution:
Below is a table that shows the catalog number suffixes for I-line breakers.
Table 9.121 represents the number system for Powerpact breakers.
Table 9.122 represents the number system for the older Legacy breakers.
The absence of a phase option suffix after a 3 pole catalog number will result in an ABC phase connection.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: