Issue:
Selection of input type on Zelio REG24 Temperature Controllers?
Product Line:
Relays and Timers
Environment:
Zelio Speed, Frequency, & Temperature Control Relays
Resolution:
Accessing the parameter
Value: Input Type
1 (PT 100 Ω )
2 (J)
3 (K)
4 (R)
5 (B)
6 (S)
7 (T)
8 (E)
12 (N)
13 (PL-2)
16 (1 VDC...5 VDC)
16 (4 mA...20 mA)
Selection of input type on Zelio REG24 Temperature Controllers?
Product Line:
Relays and Timers
Environment:
Zelio Speed, Frequency, & Temperature Control Relays
Resolution:
Accessing the parameter
1.Press the SEL key until P is displayed.
2.Press the Down Arrow key until P-n2 is displayed.
3.Press the SEL key.
6.Change the value from the default to one of the following using the Arrow keys.
Value: Input Type
1 (PT 100 Ω )
2 (J)
3 (K)
4 (R)
5 (B)
6 (S)
7 (T)
8 (E)
12 (N)
13 (PL-2)
16 (1 VDC...5 VDC)
16 (4 mA...20 mA)
Released for:Schneider Electric Canada