{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What replaces the 9065SSC10, 9065SSC20, 9065SS010, 9065SS020, 9065SS110, 9065SS120, 9065SS210, 9065SS220, 9065SS310, 9065SS320, 9065SS410, 9065SS420 overload blocks ?

Issue:
Replacement for 9065SS*** ss overload relay

Product Line:
9065SSC10, 9065SSC20, 9065SS010, 9065SS020, 9065SS110, 9065SS120, 9065SS210, 9065SS220, 9065SS310, 9065SS320, 9065SS410, 9065SS420

Environment:
NEMA and Definite Purpose Contactors and Starters

Cause:
Motor Logic Solid State Overload Relays (Discontinued)

Resolution:
Use the 9065SF type solid state overload relay instead.  Product has selectable trip class (10/20/30) on unit.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: