{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the interchangeable thermal-magnetic trip units for Powerpact H and J frame breakers?

Issue:
Do the Powerpact H and J  frame breakers have interchangeable thermal-magnetic trip units?

Product Line:
Molded Case Circuit Breaker

Environment:
Powerpact H- and J- Frame Circuit Breakers

Resolution:
Trip units can be changed on  Powerpact H, J, and L frame breakers with the T or R suffix only. Trip units without the T or R suffix cannot be changed.
Circuit breakers with interchangeable trip units are marked Line and Load and CANNOT be reverse fed.
Note that interchangeable trip units are not possible on I-Line H and J frame breakers or on 2 pole breakers.

*Available trip units for Powerpact H 60A frame
15 A  HT3015
20 A  HT3020
25 A  HT3025
30 A  HT3030
35 A  HT3035
40 A  HT3040
45 A  HT3045
50 A  HT3050
60 A  HT3060

*Available trip units for Powerpact H 100 and 150A frames
70 A    HT3070
80 A    HT3080
90 A    HT3090
100 A  HT3100
110 A  HT3110
125 A  HT3125
150 A  HT3150

*Available trip units for Powerpact J 250A frame

150 A   JT3150
175 A   JT3175
200 A   JT3200
225 A   JT3225
250 A   JT3250

Schneider Electric Canada