Search FAQs
What are the electrical ratings for NSYTRV62 terminal block?
Issue:
Needs to Identify the electrical ratings for the NSYTRV62 terminal block.
Product Line:
Linergy TR Screw terminal blocks.
Environment:
Linergy TR NSYTRV62, NSYTRV62BL
Cause:
To clarify the electrical ratings for the new line of terminal blocks compared to the old AB1 terminal blocks.
Resolution:
Terminal block NSYTRV62** have the
UL 600V, 50A
CSA 600V, 50A
ATEX 690V, 40A
All of the ratings and accessories for this terminal block is found on page 20 in the LINERGY CATALOG 9080CT1301.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: