{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why did ZB4BS84430 replace ZB4BS5430?

Issue:
Difference between trigger action and non-trigger action pushbuttons.

Product Line:
Harmony XB4/XB5 Push Buttons

Environment:
Push Buttons and Operator Interface

Resolution:
Trigger action pushbuttons are impossible to partially engage the contacts.  The trigger action causes the operator to snap over from one state to the other once engaged past a point of no return.  For safety applications and emergency off/stop applications, this is the preferred method.  In general, trigger actuated pushbuttons are 5mm longer than the non-trigger action counterparts. PDF copy of original letter sent to customer base attached.

Schneider Electric Canada

Attachment(s)
Emergency Stop Evolutions.pdf [55 KB]