Search FAQs
How do you set up preset speeds on the ATV32 drives?
Issue:
Preset speeds configuration on the ATV32 drives
Product Line:
Altivar ATV32
Environment:
All
Cause:
Preset speeds for controlling the speed
Resolution:
FULL menu enter
FUn menu enter
PSS menu enter
PS2= 2 preset speeds assign to your logic input
PS4= 4 preset speeds assign to your logic input
PS8= 8 preset speeds assign to your logic input
PS16= 16 preset speeds assign to your logic input
Preset speed values are SP2 thru SP16 in hz.
Example 3 speeds you will need to assign 4 preset speeds
LI4 preset 2 preset speeds
LI5 preset 4 preset speeds
Logic will be as follows
LI4=0 LI5=0 Drive runs at low speed for follows your analog input.
LI4=1 LI5=0 Drive runs at speed 2
LI4=0 LI5=1 Drive runs at speed 3
LI4=1 LI5=1 Drive runs at speed 4