{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What solid neutral kits can be used with the L600AWK circuit breaker enclosures?
Issue:
Application

Product Line:
Circuit Breaker Enclosure

Resolution:
There are several options for solid neutral kits for use with the L600AWK:

SN400LA for up to 400 A applications. Accepts Al or Cu conductors
SNC400LX for up to 400 A applications. Accepts only Cu conductors
SN1000MA for up to 600 A applications. Accepts Al or Cu conductors
SNC800LX for up to 600 A applications. Accepts only Cu conductors

For Ground Fault Breaker Applications:
SN600LXCT for up to 600 A applications. Accepts only Cu conductors and requires the use of the neutral current transformer (purchase neutral CT separately, S432575)

NOTE: No 200% rated neutral is available for the L600AWK

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: