{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the filter used inside the louver vent of NEMA 3R switchboards?
Issue:
Air filter for door assemblies

Product Line:
NEMA 3R enclosed Switchboards

Environment:
Products sold in North America

Resolution:
Use part number 80233-145-**.  Complete the last two digits for the part depending on size required . See table below to find the correct suffix :


filter

Schneider Electric Canada